This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G66: Frequency response of SN74LVC1G66

Part Number: SN74LVC1G66


Hi team,

For the frequency response of SN74LVC1G66, in our datasheet, there is only type value. show as below:

    

    Customer want to know the minimum value of the frequency response?

    Can you help to provide the it?

     Lacey 

     Thanks a lot!

  • Lacey,

    The frequency response of a passive FET switch is similar to a low pass filter.  The minimum frequency a signal switch will support is a DC signal.  The maximum frequency we put in the datasheet is the frequency that the insertion loss is -3dB below the insertion loss at DC. 

    What are you connecting to the signal switch that you are concerned with the minimum frequency? 

    Thank you,

    Adam  

  • Hi Adam,

    Thanks for your reply!

    Do you have the specific frequency respond curve of this part(SN74LVC1G66)?

    For the signal, I will ask customer for the detail.

    Lacey

    Thanks a lot!

  • Lacey,

    We do not have a frequency response curve for the SN74LVC1G66 but it will look like the low pass filter above with the -3dB point being 200-300MHz depending on the loading conditions.

    Thank you,
    Adam