For this question, consider the following connections. 1. V+ is 5 Volts. 2. IN is at 5V. 3. COM is at GND. 4. NC is not connected. The question is: What is the approximate switch resistance between NO and COM in the Voltage range of -0.1 and 0.0 Volts? Would the current limitations be the same in that range as it is for a Voltage in the range of 0.0 to 5 Volts?