Hi,
A customer is evaluating the CD74HC4051-Q1 and has a couple of questions below:
- What would be the propagation delay at Vcc=3.3V and Vee=GND?
- How is the jitter performance?
- There are also concerns over typical and max Ron values. Ron of this part has a lot of variation (at Vcc = 4.5V, Ron = 70 typ, 240 max). At typical Ron, with 25pF of output capacitance, the bandwidth is 90MHz. But at max Ron, the bandwidth drops to 26MHz. The slower rise time will increase the trigger signal jitter caused by voltage noise.
Thank you for your help,