Other Parts Discussed in Thread: TS3L501E,
Hi,
I have to realize a Mux/Demux showed in the attached picture for automatic testisting.
The two masters don't have to work simultaneously.
First of all I would like to know if I can connect two switches like in the picture.
I think that four RJ45 connectors with magnetics are mandatory.
Do I have to insert pull-up resistors or 100ohm resistors for each line pairs between the two switches?
Thanks for the support
Best Regards
Riccardo