Part Number: CD4067B
Other Parts Discussed in Thread: MSP430F6736, MUX506
Hi team,
I am working with CD4067B on a project. I am sending the select signals A,B,C,D and the inhibit signal using msp430f6736. However, I am unable to switch the input lines using the select signals. I get the output from the mux as the input it gets on line 0(pin#9) even when I change the select signals to a different number. Even if I change the inhibit signal to logic 1, the mux selects line 0 and shows me the output as the output that is on line 0.
Here is the circuit that I have connected. The inputs coming to the multiplexer are analog input lines of 0-1V range.
Is there an error in the circuit?
Could you help me out with the issue I am facing?
Thank you,
Keval