Part Number: SN74CBT3257
Other Parts Discussed in Thread: CD4053B
Hi,
I'm looking for an analog mux switch that can pass through bidirectional 3.3V logic signals while also passing through 4-5V switch signals. Current preference was towards using the SN74CBT3257. Is this a good choice? Or can you recommend a bi-directional analog switch with 3 signal paths with the following specs :
1) Supply Voltage (VCC) : 3.6V - 5V (single supply)
2) SPDT 2:1
3) 3.3V and 4-5V signals
4) Speed 3MHz max
Regards,
Leo