Part Number: SN74CBT3251
Other Parts Discussed in Thread: MUX506, SN74CBTLV3251, SN74CB3Q3251, TMUX1208
Dear sir,
There is a problem when I use multiplexer SN74CBT3251. The signal source is an 50 MHz optical receiver which convert the optical on/off to voltage high/low.
My problem is signal will attenuate after pass through two multiplexers SN74CBT3251 with increasing frequency.
When the clock frequency is up to 15 MHz, I got all low after inverter SN74LVC14AD.
Do you have any suggestions? Presently, I want to try another multiplexer SN74HC151PWR.
Thanks,
Ken