Hello,
I would like to use this part as an I2C mux and had a question regarding the pull up resistors. Figure 13 of the datasheet shows a typical I2C mux configuration, is it really necessary to have pull up resistors on every single multiplexed I2C signal? I would have thought that a single set of pull up resistors could be placed on the common path, reducing the resistor count from 8 to 2 (assuming using all 8 outputs). Is there some reason that TI recommends having dedicated pull ups for each I2C pair? Thanks.
-Chris Skalka