Hello everybody,
I would like to state that I have a circuit as shown below.
The problem which I am facing is that I cannot find out why the 16V supply is given to the gate of the MOSFET. There is a boost circuit implemented on the gate side. When the circuit is not working then only 16V are coming on the gate. So, that is why I have placed a 16V battery on the gate terminal. When the gate voltages is 16V then the output voltages is 12V, but I cannot find out why is that. In front of this MOSFET is connected a DC-DC converter which has a minimum operating voltage of 18V.
I cannot understand it.
Can anyone please help me?
Regards,