This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642: the maximum data transfer rate of TS3DV642

Part Number: TS3DV642


I can’t find the maximum data transfer rate in the TS3DV642 datasheet. But I find it described that it can apply in HDMI 2.0 with support for 4k2k up to 60Hz in page 1. HDMI 2.0 can support 18Gbps transfer rate. Is that mean TS3DV642 can support 18Gbps or is the 6Gbps as it mentioned in figure 8? Could you help to confirm it?

Can we calculate it out based on Shannon theorem (the relationship between maximum data transfer rate, signal to noise ratio and bandwidth)