This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A23157: TS5A23157 issue signal showing up on off channel

Part Number: TS5A23157
Other Parts Discussed in Thread: TMUX1072

The last recommended analog switch, there is a problem with the test

As shown below, PIN8--3.3V, PIN3, 1--GND, PIN10--PWM wave, logically PIN9 is on,

PIN2 is off, but the measured, PIN2 has waveform output, what is the reason

  • Eagle,

    It looks like you are operating the device out of spec.  You may not have signals on the I/O pins greater than the supply pin.  It looks like you have the supply set at 3.3 V and the I/O signal is 5 V.  If you increase you supply voltage to 5V or decrease your I/O voltage to 3.3 V does your issue go away? 

    If you would like to support I/O signals greater than supply, you need to look at a device like the TMUX1072 device. 

    Thank you,

    Adam