This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3T3306: Maximum Jitter of SN74CB3T3306

Part Number: SN74CB3T3306
Other Parts Discussed in Thread: LSF0102

Hello TI,

We are planning to use the voltage level translator (SN74CB3T3306) for conversion from +1.8V to +2.5V/+3.3V. And we do have Low Jitter Criteria for the signals that we are going to run through this Translator. As such there is no description available related to jitter in the datasheet of SN74CB3T3306.

So can you please let us know what is the maximum jitter that SN74CB3T3306 could add to the signal? 

An early response would be appreciated.

Regards,

Purvi