This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5MP645: MIPI/HDMI mux

Part Number: TS5MP645
Other Parts Discussed in Thread: TS5MP646, TS3DV642

Hi Sirs,

Sorry to bother you.

Does 645 have support HDMI signal?

If no, could you help us to find it?

Because we need 1:2 mux which could support MIPI & HMDI at same times.

Thanks!!

  • Shu-Cheng,

    The TS5MP645 and TS5MP646 devices will support any signal that is within the recommended operating conditions. 

    What is the MIPI and HDMI datarate per lane that you would like to support? 

    The TS5MP645 device has bandwidth of 2 GHz which we recommend will support up to ~1.5 Gbps. 

    The TS5MP646 device has bandwidth of 3 GHz which we recommend will support up to ~2.5 Gbps

    The TS3DV642 device has a bandwidth of 7GHz which we recommend will support up to ~4.5 Gbps

    The rule of thumb formula is the datarate per lane is the switch bandwidth x (2/3) = datarate per lane

    Thank you,

    Adam