Hi sir:
TS5A12301E be used as Bidirection load Switch. If the Current form Com to NC(NO) Under 0.4 A.Is it?
It means The com I will connect to Power,the NC(No) will connect to load. Or Nc(No) connect the power, the com connect the load.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sir:
TS5A12301E be used as Bidirection load Switch. If the Current form Com to NC(NO) Under 0.4 A.Is it?
It means The com I will connect to Power,the NC(No) will connect to load. Or Nc(No) connect the power, the com connect the load.
Lei,
All TI passive FET switches like the TS5A12301E are bi-directional. You may use this device as a load switch if the current is less than the abs max rating as you mention and within the recommended voltage range.
Thank you,
Adam