Hi,
I want to use the TS12A12511DCNR in our PCB;
Supply Voltage of the switch is 12V; the control signal for the switch (pin 6 "IN") is generated by an uC and is 4.5V.
According the specificartion of the TS12A12511DCNR the "on" level for the "IN" signal is minimum 5V. Are really 5V necessary to switch the TS12A12511DCNR to "on" @ 12V V or does it also work with 4.5V for the control signal? (I don't have 5V in the circuit).
Do sombody know the input circuit of TS12A12511DCNR pin 6 "IN - signal"?
Thanks in advance
Siegfried