This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTD3306C: SN74CBTD3306C VOL(max)

Part Number: SN74CBTD3306C


Hi Team,

Please help to confirm the VOL(max) of SN74CBTD3306C.

Thanks

  • Hi Daniel,

    The SN74CBTD3306C is a passive fet switch with level shifting.

    Here is the plot for input voltage versus output voltage for the device,

    There is a VOH spec due to the translation on the output voltage once the input rises above ~2.5V. The output voltage below this point is determine by the input voltage to the system.

    How are you planning to use this device in your system?