Hello ,
we are using the component in object as a switch to insert a 100 ohm resistor termination in a M-LVDS system
In attached you can see the part of schematic where we use the TS5A3166DCKR .
We have a big problem the switch doesn't close and so the termination 100R is not enabled .
The PCB is ok ; the power voltage is ok ! ; the signal enable is high !! ; anyway the switch doesn't close .
The voltage between signal TXRX+ and TXRX- is 1 V ! ( the voltage at pin 2 of TS5A3166DCKR is 0,3V and the voltage at pin 1 is 1 Volt .....)
The maximum frequency of swing signal in MLVDS is 25 MHZ .
I read the datasheet but I don't see any controindication on my use .
I'm afraid to have done a big error of type of choice of component .
Component problem number .
We habe about 16 boards with 2 component each with the same problem !
We buy components by DIGIKEY :
Please ... HELP !!
Alice Paolo Luigi
HEIDENHAIN ITALIANA S.r.l.
------------------------------------------------------
Tel. +39 0125 614432
Tel. +39 3421215620
------------------------------------------------------
HEIDENHAIN ITALIANA S.r.l.
Sede di Ivrea
Corso Vercelli, 123
I-10015 Ivrea (TO)