This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV16212: Could it work when VCC=3.3V and signal level on port A&B be 1.8V ?

Part Number: SN74CBTLV16212
Other Parts Discussed in Thread: SN74CBTLV3125

Hello,

     Since its VCC supply voltage range is 2.3V~3.6V, I give a 3.3V supply on VCC,but signals on both port A and B are all 1.8V level such as LVCMOS-18 standard IOs.

Is that OK?

Best regards,

Tang Yaosheng