Part Number: TMUX1574
Hi guys,
Customer is using TMUX1574, can you guys take a quick look at the schematic? is this back to back implementation ok?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMUX1574
Hi guys,
Customer is using TMUX1574, can you guys take a quick look at the schematic? is this back to back implementation ok?
Brain,
There isn’t anything wrong with cascading a passive FET switch but you will need to know that there will be twice the effect of on-state resistance and capacitance. The TMUX1574 is a new device with great low capacitance performance so I don’t think it will be an issue for the low speed JTAG debug signals.
In the schematics you are operating with 1.8 V supply and signals which is within the recommended operating conditions.
Thank you,
Adam