Hi,
We are looking for a single IC with multiple outputs with below requirements:
Input : 28V
Output 1: 5 V & 300 mA
Output 2: (-12 V) & 50 mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are looking for a single IC with multiple outputs with below requirements:
Input : 28V
Output 1: 5 V & 300 mA
Output 2: (-12 V) & 50 mA
Something like the LT8471?
It does not appeat that any of TI's single-chip split-rail converters does what you want.
Why can't you use two ICs?