This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4066: power supply current

Part Number: CD74HC4066

Hello,

My customer has a question about CD74HC4066.

[Q]

Could you tell me the power supply current under the following conditions?
- Vcc=8.5V
- VI=0 or 5V

They found one board with a large load current during shipping tests.
As a result of their investigation, it was judged that the power supply current of CD74HC4066 was large.
Usually 1mA, but the corresponding board was 6mA.
So they want to get the above information.

Best Regards,

Kaede Kudo