Hi,
When add a 10K pull-down resistor at pin IN, the voltage of IN is only 1.0V even the Pull-high voltage is 3.3V. Change 10K to 100K, result is the same, but voltage getting 3.3V after remove pull-down resistor.
1. What is the input resistor?
2. What value of resistor TI recommend?
3. For the initial state, TI recommend pin IN should initial high or initial low?
Thank you.
C.T.