Hello Adam,
one of my customer configured dual supply Vcc(+/-5V) schematic to get +/-4V swing output. COM should be output connected to load and NC, NO are applied from Vcc through resistor divider. IN comes from 0~3.3V 150Hz swing. so final target is to get 150Hz +/-4V swing on COM. however, the application makes unexpected overcurrent trouble. so, if Negative power supply(-Vcc) is replaced to GND, can see normal 0 ~ +4V 150Hz swing on COM.
would you review & find what the matter/error is here? attached the schematic.