Hello,
I downloaded the S-Parameter files for the TMUX136 ( http://www.ti.com/lit/zip/scdm209 ) and have integrated them into some simulations for a future design. I had a question about how the ports of this model map to the actual pins of the device. I could be overlooking some documentation, but I was unable to find any info on this mapping.
The S parameter file is a single 4 port model. This leads me to believe that each port is one of the following pins on the device (ie A1 = Port 1, B1 = Port 2, A2 = Port 3, B2 = Port 4). I just want to confirm that this is the case.
Another question I have is: are there S-Parameter files for the signal behavior between COM1 and A1 or B1, and COM2 and A2 or B2? Is the switch intended for usage in this way (ie passing signals from COM to an output, versus passing signals strictly from A to B.
Thanks!
Andrew