Part Number: SN74CB3T3384
Other Parts Discussed in Thread: TXB0108, , LSF0108, SN74LVC8T245
Hi Sir,
We are desperately looking for 3V to 5V level conversion device with 8 inputs/outputs.
SN74CB3T3384PWR part looks fine for the above application (3V power supply input, VCC).
We need bidirectional level conversion and one side device can accept a max. voltage up-to 3.15V after that it may get damaged. The other side device operates in 5V and hence we need 3V to 5V level conversion.
TXB0108 is a good solution for us, but it is dual supply and have a Tpd of 4ns when operating in 3V as VCCA. But we cannot compromise on the same. \
So please support us to resolve this issue that we can go with part SN74CB3T3384PWR.
Thanks & Regards,
Remya