Hi,
I am using TS3DV642 2:1 DVI switch in my project. It is handling all signals except +5V power of DVI connector, it is not switching +5V input from either of the 2 channels to the output.
My doubt is, if I can provide a +5V generated on my board to the output DVI channel which is connected to the display or should I route the same +5V coming from either of the 2 DVI input channel to the output display.
Regards,
Shyama