Other Parts Discussed in Thread: TS5MP646
We have a project that needs to implement 3 4lane MIPI inputs and 1 way 4lane MIPI through switch. Since there is no suitable 3:1 switch, we plan to implement 3:1 after using two 2:1 switch cascades.
Is it possible to use two 2:1 cascades (block diagram below)?
If there is a 3:1 MIPI switch to recommend, that would be great.if Without 3:1, if I use two 2:1 cascaded connections, the only thing we are not sure about is whether the chip supports the MIPI connection between the two TS5MP645 (circled in red below) (at the hardware underlying level).
Please help me confirm, thank you! MY EMAIL: summer@kstmicro.com