Other Parts Discussed in Thread: TS5MP646
Hi Adam,
My question is regarding the TS5MP646 performance passing single-ended signals through internal FETs.
Can a parallel port (pixel bus) from a DS90UB934 deserializer device be switched through the TS5MP646. I understand the TS5MP646 has only 10 channels. Can I assume the bandwidth is the same under single-ended use case and that cross-talk will not be an issue if single-ended 1.8V I/O logic is passed through these switches.
As per datasheet, obviously, this part is optimized for MIPI use case, but could it also support Parallel I/O without concern for slewing, bandwidth, crosstalk.
Thanks alot.
David