This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it OK to drive IN pins (1.8V logic high or 0V logic low) of TS5A21366 when VCC is unpowered?
The Recommended Operating Conditions and the Absolute Maximum Ratings allow the digital input to go up to 5.5 V/6.5 V, regardless of VCC.