This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4051-Q1: PIN2PIN comparison with 74HC4851PW-Q100

Part Number: CD74HC4051-Q1


Hello Team,

Can CD74HC4051-Q1 replace 74HC4851PW-Q100? The nexperia part pin 7 is NC where the VEE pin of the TI part is dedicated.

What is the function of VEE pin?

Thanks in advance.

Joern

  • Hi Joern,

    It depends how the 74HC4851-Q100 is being used in the system if the CD74HC4051-Q100 can be a suitable replacement. The VEE pin is the most negative power supply rail and is used for dual supply voltage applications.

    The 74HC4851-Q100 has an additional feature called current injection control. For a true replacement you should use the TI SN74HC4851-Q1.

    Do you have more information on how the device is used in the system?