Hello,
I want to design a transmitter and receiver switch fro acoustic radar and operate at 2250 Hz acoustic signals. The purpose of the switch is the same as the RF TR switch i.e. isolate the transmitter and receiver and fast switching. I am not getting any good material for this subject. With the available resources, I have designed one circuit. I have two issues with this circuit.
1. I need to put two power sources as an input (one from the power amplifier and another from the antenna) but it is not allowed by the software.
2. How I can validate or analyze its operation.