This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1574: What do the eye diagrams Figure 25 and Figure 26 attempt to illustrate?

Part Number: TMUX1574


E2E,

I am interested in the TMUX1574 and have some clarifying questions. Can I please get some assistance with the following questions?

  • What are Figures 25 and 26 attempting to illustrate?
  • Are there any additional block diagrams of this part? The customer would like to understand why the TMUX1574 can’t buffer.  Below is input we provided to customer: 

 From similar/older devices analog mux are implemented with pass FET architecture (NFET in parallel w/ PFET, gates tied together) represented by the classic switch in the block diagram.  If it was buffered there would be additional block representing output stage and associated configuration (push-pull, open drain, etc).  Another item is the datasheet specs RON of the switch and a buffer would present a high impedance so this would not be possible.

 

Thank you,

Adam

  • Hi Adam,

    Figure 25 and 26 in the datasheet are Eye diagrams for the TMUX1574. The eye diagrams help to highlight that the TMUX1574 can be used in high-speed communications without impacting the digital signals with a lot of jitter or distortion.

    Here is a link to the precision labs video on eye diagrams: https://www.youtube.com/watch?v=tZiKRfH2yZ4

    You are correct the TMUX1574 does not have an integrated buffer  as it is a passive fet switch as you mention.