This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3126: MDC/MDIO multiplexer

Part Number: SN74CBTLV3126


Dear Team,

May I know is this one suitable to use at MDC/MDIO multiplexer?

For 2.5V and MDC's maximum data rate is around 1MHz.

BR

Kevin

  • Hi, Kevin,

    The bandwidth is not specified for this device, so it's difficult for me to comment. Although for our families of bus FET switches (CBT-C, CB3T, CB3Q...etc), the bandwidth is typically in the range of 200 MHz, so it should support the application with no issue. 

    However, if you want to be certain, select a device with the bandwidth parameter clearly specified on the datasheet (such as the TMUX1511 or the TS3A4751 if you are looking for the 4ch. SPST configuration). 

    Regards,
    David