Hi, team
Could you please help me select a specific part number in multiplexers? here are the requirements.
1. there are 10 input signals which includes digital signals , 10V analog signals and a 5V,10Khz signal.
2. the output signal from the MUX is connected to the MCU I/O.
3. I want the I/O used in MCU should be as less as possible and the cost is as low as possible.