Part Number: TS3DV642
Dear Technical Support Team,
I have some questions about swapping.
If I use these case, it is easy to make pattern layout and place the parts.
I guess that these cases are possible because of just signal switch each pin.
However, I concern about the signal integrity when crossing the differential line.
1) Is it possible to swap the pin of MainLink signals below?
For example, connect ML_0+ to D1+
2)Is it possible to swap "+-" of MainLink signales?
For example, connect ML_0+ to D0-
3)Is it possible to use both 1)and 2)case?
For example, connect ML_0+ to D1-
■Function block
Best Regards,
ttd