Other Parts Discussed in Thread: LSF0108
Hi,
I'm having SN74CBTD3384C as a 5V to 3.3V translator in one of the schematic design. However, based on my testing, it seems that when I tried to send a signal at through the bus switch at 80MHz, the eye diagram of the signal is relatively small. I am suspecting the parasitic capacitance from the bus switch caused the eye to be small. I would need some help to interpret the specs of this part correctly.
- From the specs, it is mentioned that the I/O capacitance is typical at 12.5pF. So when the switch is on, does that mean both side of bus switch (A and B) each has a 12.5pF, or only one side? I'm capturing eye diagram at 80MHz
- From the specs, it only provides the propagation delay through the bus switch. How can I estimate the maximum operating frequency of the bus switch? And does this propagation delay changes when passing through a 3.3V signal (without translation) versus a 5V signal (with translation)?
- the on resistance of the bus switch is given when the input is 2.4V. How can I use this info to estimate the on resistance when the input is at 3.3V or 5V? I would need this information to calculate the total signal path resistance under different condition. Is there any application note on this or graph on the bus switch on resistance?