Is this device capable of reliably muxing between eMMC and uSD? If not, what's the recommended device for this application?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is this device capable of reliably muxing between eMMC and uSD? If not, what's the recommended device for this application?
Hi Saminah,
Adam's post is useful, but I'm not sure if this answers my question. Can TS3A5018 in particular be used to as mux between MCU and eMMC OR uSD in the same system?
Here's a table with clock and data rates, but other info may be needed.
Do you have access to JEDEC spec? I think JESD84-B51 is the one. They should spec max capacitance of bus and devices.
https://www.jedec.org/document_search?search_api_views_fulltext=jesd84-b51
Hi Bryan,
TS3A5018 supports bandwidth of 300MHz and supply voltage of 1.8-V to 3.6-V..
Based on the clock and data rates you shared in the table, TS3A5018 can be used to mux between MCU and uSD - I would also look at the signal voltage specifications.
Pease note we have not done any compliance testing of this device specifically with eMMC OR uSD.
Thank you,
Saminah