Other Parts Discussed in Thread: CD74HC4351, TMUX1208
In active state, how much current can an addressable latch serve?
1. Per active pin
2. Maximum output across all pins together
Note that at any given moment, when the latch operates in the memory mode, there could be more than one active pin, due to a previous operation. In such a case, for the CD74HC4351 should we derive the max current per pin? The data sheet specifies trh maximum DC Switch Diode Current for a few VEE combinations but the question is on how to divide the current when we operate all 8 pins at the same moment.
How do I infer/calculate these quantities from the datasheet? Can anyone help with a few examples kindly?
Thanks in advance,
Rahul