Other Parts Discussed in Thread: TS5A3159
Dear, support Team.
TS5A3159A has Isolation in Power-Down Mode, V + = 0.
Does this mean that voltage can be applied to the input even when there is no power supply voltage?
Absolute maximum rating input is up to Vs + 0.5V.
But this is the same as the A-less version of TS5A3159.
The characteristics of Off isolation are the same.
Best Regards
Hiroaki Yuyama