Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A5017-Q1: To Recommend 6 : 1 MUX for SPI Application

Part Number: TS3A5017-Q1
Other Parts Discussed in Thread: TS3A5017

My customer want to use MUX for FPGA access to multiple memories base on SPI communication.

Could you help to recommend  a suitable device for my customer?

 

Request specification :

Application :  LED Signage application ( MUX between FPGA and Memory )

Voltage : 3V to 3V

Channel Count : 6 :1

 

Questions :

1. Could you help to recommend a suitable MUX for 6:1 SPI protocol ?

2. We found TS3A5017-Q1 which is a 2 CH, 4 :1 switch could support SPI signal. Is it possible to using for 6 :1 SPI application ?  

3. According to TS3A5017(non-auto version) feature description, it support I2C communication not mentioned SPI. Dose TS3A5017 also could support SPI protocol ?