This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBT3253C: could you provide Junction temperature range Tj ?

Part Number: SN74CBT3253C


Hi

SN74CBT3253CDBQR is used in customer, customer want to know the Junction temperature range Tj.

in datasheet, there is no this information.

could you provide it?

thanks.

  • Hi Max,

    Please see this FAQ on how to calculate the Junction temperature. 

    The DBQ package thermal impedance in the datasheet is 90 degC/W. Based on the details in the above link, the junction temperature for SN74CBT3253CDBQR is approximately 107C.

    I would recommend using our new TMUX1209 mux as an alternative to the SN74CBT3253C . The TMUX1209 supports upgraded rail-to-rail switching, 1.8-V logic support, smaller package options and –40°C to +125°C temperature rating and has junction temp of 150C.

    Regards

    Saminah