Hi TI experts,
I'm going to use this switch to direct continuous current (output from a power supply) to either one of the two loops. As attached.
Power supply will constantly output for example 1A current.
I have two concern about this design:
1) In the datasheet, Vcom, Vno, and Vnc have to be within Vcc-5.5 to Vcc. However, the power supply will be a floating ground. I don't think they are referenced to the ground plane of the TS5A22362. Will that be an issue? If so, how should I get around with it?
2) The maximum current rating of this part is 350mA, I would have to shunt three switches in parallel to achieve this. Will there be any problem if I shunt three switches together (Vcc, COM, NO, NC nodes are combined among three switches, respectively.
Thank you for your help in advance.
Cheers,
Yixin