Part Number: TX810EVM
Do we have/can we generate a 3D CAD model for the TX810EVM?
Our customer is mocking up a system they are developing and using the EVM. (We don't need the model for the IC, that's available on the website).
From the customer:
------
We are implementing this EVM onto an experimental mother board tying together other components along with the TX810EVM. This will not be used beyond lab research to evaluate the TX810 along with other components we are evaluating. The motherboard serves no purpose other than to make the interconnections more neat and manageable and less prone to signal degradation. Any end product that may be developed would only use the TX810 IC as intended on a standard circuit board, and would not use the EVM.
This application is for development use only, but it is still critical for a mechanical layout of the electrical components. Of particular interest would be the I/O locations for our interface definition.
------