This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3126: SN74CBTLV3126PWR the value of Tj?

Part Number: SN74CBTLV3126

can you provide the valve of Tj about SN74CBTLV3126PWR?

  • Hi Simba,

    You can refer to this FAQ to calculate the Junction temperature of the device.

    I would also recommend looking at our new TMUX1511 which is p2p compatible with the SN74CBTLV3126 and has additional features like 1.8-V compatible control inputs and Fail-safe logic.

    Regards,

    Saminah