This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
And I can’t find the “SN74HC4851QPWRQ1 “HBM ESD value from the datasheet, can you help me ,thanks.
Hi Martin,
The HBM ESD information is not available in the SN74HC4851-Q1 datasheet.
What is your application and end equipment?
Have you seen the new TMUX1308-Q1? TMUX1308-Q1 is a great new 8:1 mux option with current-injection control. In addition, TMUX1308-Q1 offers improved Ron, lower leakage current, and additional features such as 1.8V compatible control inputs, break-before make switching, and a new small package SOT-23 THIN. The HBM ESD rating for TMUX1308-Q1 is +/-2000V.
Let me know what you think about TMUX1308-Q1!
Best regards,
Kate