Other Parts Discussed in Thread: TS5A3167
Hi Sir,
I want to double confirm if SN74AUC1G66 have internal pull LOW to GND in switch OFF status?
I means if trace from IN to OUT if have internal PULL LOW, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
I want to double confirm if SN74AUC1G66 have internal pull LOW to GND in switch OFF status?
I means if trace from IN to OUT if have internal PULL LOW, thanks.
Hi Ian,
When the switch is OFF (control input is LOW), the switch will be in the high-impedance state. Neither terminal (A or B) will be internally pulled to GND.
What is your application? We have many options for 1:1 switches if you are interested in a new device. However, our switches are designed to have high-impedance signal path when the switch is disabled.
Let me know if this helps.
Best regards,
Kate
Hi Kate,
This application is block DC bias(around 1~1.8V) in audio signal path.
Do we have better solution for kind of application?
Thanks, Ian.
Hi Ian,
All of our analog 1:1 switches will be in the high-impedance state when disabled by the control logic. Will this be compatible with your system?
There are quite a few options for single channel 1:1 switches. Check out this link to the parametric search tool to sort by parameters and features.
A feature you may be interested in is powered-off protection, which ensures that the switch is in the high-impedance state when there is no power supplied to the device. Take a look at TS5A3167, which can be used in audio applications. TS5A3167 has lower Ron, lower leakage current, and includes the powered-off protection feature. The DBV (SOT23) package is pin-to-pin compatible (but the control pin logic is opposite - the switch is ON when control is LOW).
Let me know what you think about TS5A3167.
Best regards,
Kate