Other Parts Discussed in Thread: LM2904
Hi,
We are using the TS12A12511 to choose -5V and -3V to control Gate voltage of GaN MOS.
NC is -5V, NO is -3V. V- is -5V, V+ is 5V. IN is 0V and 3V change.
In theory, the COM should be -3V and -5V controlled by IN.
But you can see below signal. It is normal when -3V changed to -5V. But when -5V changed to -3V, there is -4.5V in the meanwhile.
Can you help resolve this issue?
Thanks
Saminah