This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3257: SPI up to 50MHz

Part Number: SN74CBTLV3257


Dear Team,

Can this device support SPI interface up to 50MHz?

If no, please suggest one to replace SN74CBTLV3257PWR

BR

Kevin

  • Hi Kuan,

    For digital applications we recommended the switch bandwidth be 1.5 times the datarate per lane or 3 time the clock frequency per lane.  

    The SN74CBTLV3257  with 200MHz bandwidth should be ok to support SPI up to 50MHz. However, I would also recommend the new TMUX1574 p2p compatible with  SN74CBTLV3257PWR,  also supports SPI signals along with wide operating voltage, high bandwidth, additional features like 1.8-V compatible control inputs, Fail-safe logic.

    Thanks

    Saminah