This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1219: 1.1A continuous current on contact pins

Part Number: TMUX1219
Other Parts Discussed in Thread: TS5A12301E, TS5A6542, TPS2111A

Hi Team,

Our customer is asking for an alternate solution for TMUX1219. Their set-up requires a switching between S1 and S2 on two voltages (3.3V and 3V) as tests are conducted on the circuits further down the chain. When the first switching occurs, there could be as much as 1.1A running through the connection - which is way to high for TMUX1219.

We've checked for several solutions but the highest continuous current SPDT switch we've found is only rated at 450mA (TS5A12301E and TS5A6542). Would you able to give us other possible solutions our customer can consider? Thank you very much in advance.


Kind Regards,

Jejomar