Part Number: SN74CBT3384A
I've designed a component video + audio switch using the SN74CBT3384ADWR. Unfortunately, while either switch / both switches are in the 'off' state (~OE pin high) there's a lot of signal bleeding through. If the Luma signal is especially high-value (white screen), the signal will make it through to the other side. Same thing for loud audio signals; it bleeds through and is very noticeable. I'm operating within the recommended spec for voltage supply (4.7v is what I measure as I type this) so I would wonder if there's something wrong with all six of my SN74CBT3384ADWR? Perhaps there's some other minutia I don't understand yet?
If it's of any concern, the ~OE pins are being driven by the output of a pair of D-latches (SN74HCT74DR) and there is also an LED's cathode connected to either ~OE pin through a 20K resistor (anode connected to VCC) for visual feedback.